Activities Tree - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
Note: The Activities tree was previously called the Application Logic tree.

The Activities tree appears at the top of the left panel in the logic view. This selection tree allows you to view the logic for the entire application, or select to view the logic of an individual module.

To view the logic of the entire application, click the Control View Connections option (appears second in the list, just below the Activities folder). The logic of the entire application appears in the right panel of the logic view. The Control Block Palette does not appear when the Control View Connections option is selected.

Note: By default, the Control View Connections option is selected when you first click the Logic tab.

To view the logic of a particular module, browse the folders of the Activities tree (organized by module category) and click the desired module. The logic diagram of the module appears in the right panel and the Control Block Palette appears below the Activities tree in the left panel.