Logic Tab - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Logic tab allows you to view and modify the control logic used in your system. This view displays the logic blocks visually to provide information about your system. Depending on the mode in which the tool is operating, you are able to perform certain tasks in the Logic tab. For information on the modes, see the Modes section.

The following figure shows the Logic tab in the Classic View workspace, and the table describes the components.

Figure 1. Logic Tab

Table 1. Logic View Screen Details

Callout

Screen Area

Description

1

Toolbar

Icons for the actions you can perform in the Logic View.

2

Activities Tree

Contains a tree view that allows you to view the logic for the entire application, or select to view the logic of an individual module. See the Activities Tree section.

Note: The Activities tree was previously called the Application Logic tree.

3

Control Block Palette

Contains a tree view (folders) of the blocks to drag and drop into the logic diagram and the Launch Wizard search feature. See the Control Block Palette and Launch Wizard sections. The Control Block palette does not appear when viewing logic of the entire application (Control View Connections option of the Activities tree).

4

Logic Diagram

Displays a graphical representation of the selected module’s logic. See the Logic Diagram section for information on the diagram and its components.

5

Features Panel

See the Features Panel section for information on this panel.

Table 2. Logic Tab Tasks Available in Different Modes

Task

Mode

Configuration

Simulation

Commissioning

View Logic

X

X

X

Use the Launch Wizard

X

   

Add Blocks

X

   

Rename Blocks

X

   

Modify Blocks and Their Details in the Details Dialog Box

X

X

X

Delete Blocks

X

   

Connect Blocks

X

   

Align Blocks

X

   

Show/Hide Connection Lines

X

   

Delete Connections

X

   

Export a Module

X

   

Send a Command

 

X

X 1

Select Default Element

X

   
1 Applies to test mode.