Miscellaneous (Inputs) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This module category appears on the left side of the Control tab below the Inputs category (Figure 1). These modules are used for override monitoring. A miscellaneous input reads the current Present Value and Priority of PAO, AO, and BO objects.

Note:

Override monitoring is not available during Simulation mode.

See Miscellaneous Input Modules for information.

Back to Control Tab Module Categories