Inputs - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Inputs category appears in the Control tab. This section lists the inputs defined for the system. An input defines an interface to the actual hardware in a system. An input can represent a physical sensor in the system or an input associated with a sensor. Inputs get data directly from hardware input points of a device.

During simulation and commissioning modes, the Input category displays a second row of text. This row provides the Input present value.

See Input Modules for information.

Back to Control Tab Module Categories