System Upgrade (with Modules) Screen - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

See Upgrading a System.

Table 1. System Upgrade (with Modules) Screen

Field

Description

Version Information

Displays tool version information.

Standard Modules

Modules that require upgrade.

User Modified Modules

Modules that have been modified by a user. User-modified modules are not included in the upgrade.

Yes

Closes the System Upgrade screen and upgrades the CAF and modules.

No

Closes the System Upgrade screen and does not upgrade the CAF and modules.

Help

Opens the Help system.