Table 1 lists and describes the new modules that have been added to the system since the last release.
|
Module |
Description |
|---|---|
| Damper Command OR |
Output Control: Provides OR logic for damper control. |
| Exhaust Damper Control |
Output Control: Provides control logic for the exhaust damper position in flow control modules, based on the VAV-Supply Damper Control v51 module. |
| Slave Supply Flow Setpoint Control HFR |
Output Control: Provides flow setpoint controlled by the Supply Damper Control module. This module uses a heating flow reset strategy. |
| Secondary Bypass Valve Sequencing |
State Generation: Provides control logic for secondary bypass valve PID, based on system enable and output of the secondary pumping PID. |
| Application Mode Override |
State Generation: Enables user to override the current AHU operation mode. |
| Status AND |
Setpoint/Miscellaneous: Provides AND logic for the dual pump status. |
| N2 VAV DD Common Outputs | Output Control: Translates the controllers' cooling control status commands into the outputs required for the legacy application. |
| N2 Terminal Mode Input | Setpoint/Miscellaneous: Translates the N2 mode commands into the outputs required for the legacy application. |
| N2 VMA DD Mode Input | Setpoint/Miscellaneous: Translates the VAV Dual Duct Box Mode, Water Flush, Warmup Command, and Cooldown Command into outputs required for the legacy application. |