Bulk CAF Upgrade Utility - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Bulk CAF Upgrade Utility allows you to upgrade multiple CAFs at once. The CAFs must reside on the same computer as the tool. The utility upgrades the selected CAFs to the current version of the tool, including changes to system selection default selections and any necessary updates to the modules defined within the files. The tool upgrades any PID and PID Pre-Processor blocks located within the application.

See the Upgrading Multiple Systems Using the Bulk CAF Upgrade Utility and the Bulk CAF Upgrade Utility Dialog Box sections for more information.