Backup Files - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

When you upgrade your system, the tool creates a backup version of the original file and stores the file in the same directory as the original file. The backup file has the same name as the original file; however, the backup file has a .bak extension. To use the backup file, you need to remove the extension from the file name.

Note: The default location of a CAF is C:\Users\username.