Optional Equipment (UV) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The selection options for Optional Equipment are:

  • Filter Switch: This option creates a Filter Status Input that is typically mapped to the Supervisory system to create a Change Filter Alarm.

  • Lighting: An output to interface a Lighting Relay is created if the Lighting Selection is checked. If the lighting option is selected, the Always Occupied selection in the Occupancy (UV) section is not available. Only the Occupancy Mode Determination Mode logic interfaces with the Lighting Output. The default output configuration is a single maintained binary output.