Economizer Suitability (UV) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Economizer Suitability selections are not available when ASHRAE Cycle 1 is selected. Otherwise, the Economizer Availability Determination Setpoint module is created and interfaced to the choice selected.

The selection options for Economizer Suitability are:

  • Network Command

  • Binary Input (Enthalpy Switch)

  • Outdoor Air

    • Dry Bulb Temp Economizer

    • Temp & Enthalpy Economizer