Unit Ventilator Applications - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Unit Ventilator application provides mechanical and control logic selections that match ASHRAE cycles for standard Unit Ventilator configurations.

See the Upgrading System Files section for a list and description of the module and System Selection changes that were made since the last release of the tool.