|
Field |
Description |
|---|---|
|
Connection Screen |
|
|
Connection Type |
Select the type of connection to use:
|
|
Connection Parameters |
NxE Passthru: Enter the connection parameters
required to connect to the supervisory device. If you are connected to an SCT archive, do the following:
For all modes, the following connection parameters are required:
Note: To use the NxE Passthru connection, you do not need to launch the
tool through the supervisory device configuration tool or user interface, or have
the supervisory device configuration tool installed. When you launch the tool from
the supervisory device configuration tool, the supervisory device connection
information is not automatically populated in the tool.
|
| Bluetooth: Specify the COM port and baud rate to use. | |
MAP 4.2+ / BACnet Router: Use to specify the following:
When you first open the wizard, the default connection parameters for connecting to a MAP Gateway at version 4.2 are automatically displayed. If the connection parameters are modified, the values are stored in the wizard for future use. To restore the connection parameters to the default values, click the MAP 4.2 Default button. For further information about the MAP and common troubleshooting issues, refer to the Mobile Access Portal Gateway User's Guide (LIT-12011999). |
|
| ZigBee: Specify the personal area network (PAN) Offset. | |
| Direct Ethernet: Specify the UDP port of the device and an available network interface. Select a network interface that is connected to the same subnet as the IP controllers to which you want to connect. | |
|
Discovery |
Indicates the type of discovery process to use:
|
|
Device Selection Screen |
|
|
Discover |
Use this feature to perform a device Discovery over the network to find a device.
The Discovery option only returns field devices and I/O Modules that are on the
Field Bus.
Note: After a Discovery completes and you click Discover again,
the list clears from the Device Selection table.
|
|
Stop |
Stops the Discovery process. |
|
Devices Table |
Displays available devices, including:
Note: The first column (no header name) indicates the number of devices
discovered.
|
|
Transfer Summary Screen |
|
|
Device Information |
Displays the following device information:
|
| Device Information (contd.) |
|
|
SA Bus Status |
Click this option to view the status of all SA Bus devices. The SA Bus Status Screen lists the status of each device detected by the controller on the SA Bus. For each device detected, it shows the status of files (such as Boot and Main), the device version, and the version the controller has for provisioning that device. In the Online Operations (Comissioning mode), Transfer to Device, and Commission Device (Current Application) wizards, this feature displays the status of defined SA Bus devices in a CAF and identifies devices that are defined in the application, but not reported by the controller. This information can be used to verify that the controller has connected to the correct equipment for the application. Note: The availability of this feature depends on the firmware of the device, and
some device types may not be reported. Refer to controller product documentation
for more information.
|
|
Operations |
Displays the following Transfer Operation options: After transfer Transferred files are activated after the Transfer to Device (Download) process completes. Wait for manual activation Transferred files are not activated when the transfer process completes. You must manually activate the transferred file using the Activate pending files action in Tools > Online Operations. See the Online Operations Wizard for more information. Enable logic On supported devices, enables the runtime logic of activated files. Disable logic On supported devices, disables the runtime logic of activated files. If you choose to disable the logic of an application, you can enable it later by selecting the Enable logic action in Tools > Online Operations. See the Online Operations Wizard for more information. |
|
Advanced Transfer Options |
Click to display the following transfer code types: Following advanced transfer options: Modify open application with New Information column Updates the CAF with the changed values in the New Information column upon
Transfer.
Note: If you select this feature the Controller Number also
updates.
Close wizard after successful transfer Closes the Transfer to Device wizard after successfully completing the operation. Commission device after successful transfer View the device in Commissioning mode after successfully completing the
operation.
Note: This option requires you to select the
Modify open
application with New Information column
option if it is available.
Override Maximum System Capacity This operation only appears if you are working with large CAFs that exceed the controller's supported size. You must check this operation when it appears to proceed with the application transfer. |
| Status | Transfer status. |
|
Previous |
Moves to the previous screen of the wizard. |
|
Next |
Moves to the next screen of the wizard. Note: This option is disabled if a device with a duplicate Instance Number is
selected.
|
|
Finish/Done |
Click Finish to start the transfer. Click Done to close the wizard. |
|
Cancel |
Closes the wizard without performing the transfer. |
|
|
Opens the Help system. |
1 Appears only for compatible
devices.
2 Appears only for IP devices.
3 Appears only when wirelessly
connected.
4 This option only appears when the device is
in wireless mode. See the Radio Code description in the Code File Types
section.
5 The
Switch Communication Mode option appears when you must switch controller
communication protocols to ensure application compatibility. If you do not
switch communication modes, you cannot transfer the application. For
information about N2 communication switching see the Switch
Communication Mode Workflow section. This step is not necessary if
the device supports background transfer, as the transfer of N2 applications to
such devices does not require explicit communication switching.
6 This feature is only
available to devices that support SA Bus Provisioning.