|
Connection Screen
|
|
Connection Type
|
Select the type of connection to use:
- NxE Passthru
- Bluetooth
- MAP 4.2+ / BACnet Router
- ZigBee
- Direct Ethernet
|
|
Connection Parameters
|
-
NxE Passthru:Specify the following:
-
Host Name/IP Address: The device host name or IP Address.
-
User Name: Credentials to log into the site.
-
Password: Credentials to log into the site.
-
Supervisory Device: The supervisory device to use for the NxE Passthru connection.
-
Trunk: The trunk to use for the NxE Passthru connection.
Note:
To use the NxE Passthru connection, you do not need to launch the tool through the supervisory device configuration tool or user interface, or have the supervisory device configuration tool installed. When you launch the tool from the supervisory device configuration tool, the supervisory device connection information is not automatically populated in the tool.
Bluetooth: Specify the COM port and baud rate to use.
-
MAP 4.2+ / BACnet Router: Use to specify the following:
- IP address and UDP port of the router.
- Network number of the MS/TP trunk (1-65,534).
Note: Do not use 1001 for the MS/TP Network Number. The MS/TP Network Number 1001 is reserved for Johnson Controls IP network connections.
- An available Ethernet network interface adapter to use.
Note: If you select an available Ethernet network interface, all IP traffic intended for the MAP 4.2+/ BACnet Router travels through this interface.
When you first open the wizard, the default connection parameters for connecting to a MAP Gateway at version 4.2 are automatically displayed. If the connection parameters are modified, the values are stored in the wizard for future use. To restore the connection parameters to the default values, click the MAP 4.2 Default button.
Note: For further information about the MAP and common troubleshooting issues, refer to the Mobile Access Portal Gateway User's Guide (LIT-12011999).
-
ZigBee: Specify the PAN Offset.
-
Direct Ethernet: Specify the UDP port of the device and an available network interface. Select a network interface that is connected to the same subnet as the IP controllers to which you want to connect.
|
|
Discovery
|
Indicates the type of discovery process to use:
- Auto
- MAC Address
- Instance Number
- IP Device (when Bluetooth is selected)
|
|
Device Selection Screen
|
|
Discovery
|
Use this feature to perform a device Discovery over the network to find a device. The Discovery option only returns field devices and I/O Modules that are on the Field Bus.
Note: After a Discovery, when you click Discover again, the list clears from the Device Selection table.
|
|
Stop
|
Stops the Discovery process.
|
|
Devices Table
|
Displays available devices, including:
- Device Name: Name of the device.
- System Name: Name of the system.
- Address: Address of the device. You can sort on this column.
- Type: Type of device.
- Status: Status of the device.
- Instance Number: TheBACnet ID number. This value is the same value used in the Peer Reference attribute in the Details View.
- Controller Number
1: Combined value of the rotary switches or DIP switches on the device.
- Computer Name
2: Network hostname of the device.
- IP Address2: IP Address of the device.
Note: The first column (no header name) indicates the number of devices discovered.
|
|
Transfer Summary Screen
|
|
Device Information
|
Displays the following device information:
- Computer Name2: Network hostname of the device.
- Instance Number: BACnet ID number. This value is the same value used in the Peer Reference attribute in the Details View.
- DHCP-Enabled Check box: Enables or disables the dynamic IP address.
When the DHCP Check box is disabled or not checked, the static IP fields are editable.
-
IP Address2: IP address of the field device.
-
IP Mask2: Subnet mask used for the IP address.
-
IP Router Address: IP address of the router for the field device.2
- BBMD Enabled: Configures the Enabled attribute of the Broadcast Management (BBMD) object located in the Advanced tab. For further information, see Broadcast Management (BBMD) Object Screen.
- Controller Number1: Combined value of the rotary switches or DIP switches on the device.
- Name: Device name.
Note: The default device name is the same as the System Name. The Device Name can be changed from the Advanced tab of the Device Object.
- Description: Description of the device.
- Model: Model number of the device.
- Boot Code Version: Boot Code version.
- Main Code Version: Main Code version.
- System Name: System name.
- CPU Usage: CPU usage.
- Object Memory Usage: Memory used by the objects in the device.
- Status: Device’s status.
- Radio Firmware Version
3: Firmware version of the wireless devices.
- Radio IEEE Address3: IEEE address of the wireless devices.
- Pan ID3: Pan ID of the wireless devices.
- Device Address2: Address of the device.
- Unbound References: Unbound references of the device.
- FC Communication Mode: On compatible devices, indicates the following field bus communication: N2 Slave, Wired, Wireless, and Ethernet.
|
|
Device Information
(contd.)
|
- Logic Enabled: The logic status of an
application configured in
Transfer to Device
(Download)
. A status of True indicates
that the logic of an application is enabled; a status of
False indicates that the logic of an application is
disabled. To modify the Logic Enabled status, see Online
Operations.
Note: The logic options do not take effect on the controller until the
application is activated.
- Background Transfer Status: The
status of an application transferred using the
Transfer to
Device (Download)
option. A status of Idle
indicates that the application is activated in the controller; a status of
Files are Staged indicates that the application has yet
to be activated. To activate pending files, see Online Operations.
- SA Bus Status: Click this option to
view the status of all SA Bus devices. See Transfer to Device Wizard for more information.
|
|
Operations
|
The Code type and Status of the transfer. |
|
Status
|
The transfer status. |
|
Previous
|
Moves to the previous screen of the wizard.
|
|
Next
|
Moves to the next screen of the wizard.
Note: This option is disabled if a device with a duplicate Instance Number is selected.
|
|
Finish/Done
|
Click Finish to start the transfer.
Click Done to close the wizard.
|
|
Cancel
|
Closes the wizard without performing the transfer.
|
|
|
Opens the Help system.
|