The following table describes the attributes used by the WarmupCooldown Sequencing module.
|
Name |
Description |
Default Value |
|---|---|---|
|
Box Heating Control Status |
Contains the current control status from the box heating controller necessary for the sequencer to determine what actions to take. |
Overridden Set Name: Control Status |
|
Heating Priority |
Defines whether supplemental or box heat should be the next level of heat after the primary heat has been used. |
Supplemental Set Name: VAV Heating Priority |
|
Heating Setpoint |
Contains the desired setpoint for the zone temperature when under warmup control. |
21 °C, 70 °F |
|
Mode |
Supports a network command for Warmup, Cooldown, or Coast. |
Normal Set Name: OST Warmup Cooldown |
|
Primary Heating Control Status |
Contains the current control status from the Supply Flow Setpoint Control necessary for the sequencer to determine what actions to take. |
Overridden Set Name: Control Status |
|
State |
Contains the current state generated by Warmup Cooldown Sequencing. |
Set Name: VAV Warmup Cooldown State |
|
Supp Heating Control Status |
Contains the current control status from the supplemental heating controller necessary for the sequencer to determine what actions to take. |
Overridden Set Name: Control Status |
|
WC-STATE (WarmupCooldown Status) |
Contains the desired status of WarmupCooldown. This output is the default element as it is the key output of this module typically connected to the State Selection. |
Set Name: VAV Warmup Cooldown Status |
|
Zone Temperature |
Specifies the process variable. |
22 °C, 72 °F |