Attributes (WarmupCooldown Sequencing) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following table describes the attributes used by the WarmupCooldown Sequencing module.

Table 1. WarmupCooldown Sequencing Attributes

Name

Description

Default Value

Box Heating Control Status

Contains the current control status from the box heating controller necessary for the sequencer to determine what actions to take.

Overridden

Set Name: Control Status

Heating Priority

Defines whether supplemental or box heat should be the next level of heat after the primary heat has been used.

Supplemental

Set Name: VAV Heating Priority

Heating Setpoint

Contains the desired setpoint for the zone temperature when under warmup control.

21 °C, 70 °F

Mode

Supports a network command for Warmup, Cooldown, or Coast.

Normal

Set Name: OST Warmup Cooldown

Primary Heating Control Status

Contains the current control status from the Supply Flow Setpoint Control necessary for the sequencer to determine what actions to take.

Overridden

Set Name: Control Status

State

Contains the current state generated by Warmup Cooldown Sequencing.

Set Name: VAV Warmup Cooldown State

Supp Heating Control Status

Contains the current control status from the supplemental heating controller necessary for the sequencer to determine what actions to take.

Overridden

Set Name: Control Status

WC-STATE (WarmupCooldown Status)

Contains the desired status of WarmupCooldown. This output is the default element as it is the key output of this module typically connected to the State Selection.

Set Name: VAV Warmup Cooldown Status

Zone Temperature

Specifies the process variable.

22 °C, 72 °F