Module Use in Applications (Staged Device Enable Determination Series) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual module in this group using the name in the following table.

Table 1. Staged Device Enable Determination Series Uses in Application System Selection Trees

Module Instance Name

Applications

VAV Flow Determination

VAV Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.