Attributes (Staged Device Enable Determination Series) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The following table describes the attributes used by the Staged Device Enable Determination Series module.

Table 1. Staged Device Enable Determination Series Attributes

Name

Type 1

Description

Default Value

Fan Mode

 

Indicates whether the fan is currently commanded on.

Off

Set Name: Off/On

Staged Device Min Flow

 

Indicates the minimum required flow before issuing a command to true without the fan being commanded on.

100.0 | 200.0

Display Units: l/s | cfm

State

G

Provides the desired status to Staged Enable.

False

Set Name: False/True/Fault

Supply Flow

 

Indicates the measured supply flow.

0.0

Display Units: l/s | cfm

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)