Staged Device Enable Determination Parallel - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Staged Device Enable Determination Parallel module ensures that airflow is enabled before VAV Staged Box Heating Control is enabled. The module interlocks with a parallel fan command, or checks that the supply flow is greater than the minimum heating flow setpoint (when there is a box fan) before enabling the staged heating.