Module Use in Applications (Balancer Override) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Balancer Override Uses in Application System Selection Trees

Module Instance Name

Applications

Balancer Override DD

VAV Dual Duct Applications

VAV Slave Dual Duct Applications

Balancer Override DDX

VAV Dual Duct Applications (with exhaust box)

VAV Slave Dual Duct Applications

Balancer Override SD

VAV Single Duct Applications

VAV Slave Single Duct Applications

Balancer Override SDX

VAV Single Duct Applications (with exhaust box)

VAV Slave Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.