Reliability (Fan Determination [VAV Series]) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This module always uses the last reliable value received if any of the inputs should become unreliable. The default value of the input is used if the signal to it has never been reliable.