Unit Enable Determination - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This module generates a unit enable command. This command is generated from a combination of a network and hardware mode and the parameters for controlling the power fail restart.

You can view and modify the modules in this group’s logic.