System Mode Determination - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Terminal Unit applications have a System Mode input that allows you to force the unit into a mode of operation. The possible modes are Cool Only, Heat Only, Fan Only, Water Flush, Purge, and Auto. This module splits out the Water Flush mode to a separate output to allow it to be separately connected to State Selection.

You can view and modify the modules in this group’s logic.