Primary States (System Mode Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
  • Cool Only: The unit may operate but cannot use heating devices.

  • Heat Only: The unit may operate but cannot use cooling devices.

  • Fan Only: The unit may operate but cannot use heating or cooling devices.

  • Purge: The unit should start and operate with maximum outdoor air but no heating or cooling devices.

  • Auto: There are no system mode overrides.