System Mode Determination - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Terminal Unit applications have a System Mode input that allows you to force the unit into a mode of operation. The possible modes are Cool Only, Heat Only, Fan Only, Water Flush, Purge, and Auto. This module splits out the Water Flush mode to a separate output to allow it to be separately connected to State Selection.

You can view and modify the modules in this group’s logic.