Attributes (Occupancy Mode Determination) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The following table describes the attributes used by this module.

Table 1. Occupancy Mode Determination Attributes

Name

Type 1

Description

Default Value

EFF-OCC (Effective Occupancy)

G, V

The resultant Occupancy Mode of the control system as determined based on the input values.

Set Name: Occ Effective

OCCMODE-BYPASSTIME (Bypass Time)

V

Length of time that the Bypass mode remains active, once activated.

3600 Seconds

Occupancy Override

SC

Contains the highest priority in controlling the effective occupancy output. It typically is controlled by the user directly commanding the input.

Not Set

Set Name: Occ Override

Occupancy Schedule

SC

Contains the third highest priority in controlling the effective occupancy output. It typically is controlled by a schedule in the supervisory system.

Not Set

Set Name: Occ Schedule

Occupancy Sensor

SC

Indicates when someone is in the space or whether the space should be considered occupied.

Not Set

Set Name: Occ Sensor

Temporary Occupancy

SC

Represents a local momentary button that allows occupants to indicate their presence.

Inactive

Set Name: Inactive/Active

State

V

Indicates which input is presently driving the Effective Occupancy

Occupancy Override

Set Name: Occupancy Effective State

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)