Occupancy Mode Determination (MZ) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This module extends the base Occupancy Mode Determination module with support for a Temporary Occupancy input for up to eight zones (with the zone number designated here by X, representing zones 1-8). You can view and modify this module; however, you cannot change the key behavior performed by the Occupancy Mode Determination module.