|
Input |
Behavior When Input Is Not Reliable |
|---|---|
|
Hardware Mode |
Specifies that when the Hardware Reliability is False the State output matches the Network Mode if the Network Reliability is True. If both Hardware Reliability and Network Reliability are False, the output is Normal. |
|
Network Mode |
Specifies that when the Network Reliability is False the State output matches the Hardware Mode if the Hardware Reliability is True. If both Hardware Reliability and Network Reliability are False, the output is Normal. |