The following table describes the attributes used by the Energy Hold Off Determination modules.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
EHO-STATE (State) |
G, V |
Contains the state output generated from the Network mode and Hardware mode inputs based on the Resolution Mode setting. |
Set Name: Normal/Energy Hold Off |
|
Hardware Mode |
Specifies whether to allow the unit to operate normally or in Energy Hold Off. |
Normal Set Name: Normal/Energy Hold Off |
|
|
Network Mode |
Specifies whether to allow the unit to operate normally or in Energy Hold Off. |
Normal Set Name: Normal/Energy Hold Off |
|
|
Resolution Mode |
Used when both inputs are connected to determine how the two input commands (network and hardware) should be resolved into a single output command. |
Either Can Activate Set Name: Resolution Mode |