Energy Hold Off Determination - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This module resolves two energy hold off inputs, one hardware mode and one network mode, into a single energy hold off output. This single output is generated from the two inputs based on the resolution mode setting and the reliability of the inputs. Energy Hold Off is typically used with Zone Low Limit Determination for applications serving zones with direct openings outside the building, including loading docks and offices with operable windows. When the Energy Hold Off is active (that is, window open), all heating and cooling is de-activated. The Zone Low Limit option should be selected if heat is needed to prevent the zone from cold outdoor air conditions.

You can view and modify the modules in this group’s logic.