Primary States (Application Mode Determination) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
  • Cool Only: The unit may operate but cannot use heating devices.

  • Heat Only: The unit may operate but cannot use cooling devices.

  • Fan Only: The unit may operate but cannot use heating or cooling devices.

  • Purge: The unit should start and operate with maximum outdoor air but no heating or cooling devices.

  • Vent: The unit should start and operate with maximum outdoor air as well as any available heating or cooling devices.

  • Auto: No application modes are active.