Attributes (Application Mode Determination) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The following table describes the attributes used by the Application Mode Determination modules:

Table 1. Application Mode Determination Attributes

Name

Type 1

Description

Default Value

Application Mode

 

Indicates the current Application Mode.

Auto

Set Name: AHU Application Mode

Eff Mode

G, V

Indicates the effective Application mode after splitting off the Water Flush output.

Set Name: AHU Effective App Mode

Water Flush

V

Indicates whether Water Flush is requested.

Boolean

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)