Module Use in Applications (Pass Through) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Pass Through (Boolean, Enum) Uses in Application System Selection Trees

Module Instance Name

Applications

Condensate Alarm Pass Through

All Air Handling Unit Applications

Fan Coil Applications

Heat Pump Applications

Unit Ventilator Applications

Emergency Mode Pass Through

No longer used. Previously used by:

Heat Pump Applications

Unit Ventilator Applications

VAV Single Duct Applications

VAV Dual Duct Applications

Fan Control by Others BI Pass Through

Fan Coil Applications

Heat Pump Applications

Unit Ventilator Applications

Fan Speed Override Pass Through

Fan Coil Applications

Heat Pump Applications

Unit Ventilator Applications

Master CD Constant Flow Setpoint Pass Through

VAV Slave Dual Duct Applications

Master CD Flow Setpoint Pass Through

VAV Slave Dual Duct Applications

Master Flow Setpoint Pass Through

VAV Slave Single Duct Applications

Master HD Flow Setpoint Pass Through

VAV Slave Dual Duct Applications

WarmupCooldown Pass Through

All Air Handling Unit Applications

Fan Coil Applications

Heat Pump Applications

Unit Ventilator Applications

Water System Flush Pass Through

All Air Handling Unit Applications

Fan Coil Applications

Unit Ventilator Applications

VAV Single Duct Applications

VAV Dual Duct Applications

Waterside Economizer State Pass Through

Central Cooling with Optimization Applications

Zone Damper Mode Pass Through SG v50

AHU Multizone (Mixed Air Dual Duct) Applications

Zone Htg Valve Mode Pass Through SG v50

AHU Multizone (Mixed Air Dual Duct) Applications

Zone Staged Htg Mode Pass Through SG v50

AHU Multizone (Mixed Air Dual Duct) Applications

A pass through module takes a value from a Network Input and connects it to State Selection.

To see a module's connections and how modules interact with it, view the Connections table.