Primary States (Occupied Zone Sequencing [VAV] HFR) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
  • Satisfied: The sequencer is in this state when Heating or Cooling are not needed.
  • Supp Htg: The sequencer is in this state when the Zone Temperature is less than the Heating Setpoint and Box Priority = Supplemental.
  • Supp Htg + Box Htg: The sequencer is in this state when the Zone Temperature is less than the Heating Setpoint, Box Priority = Supplemental, and Supp Heating Control Status = High.
  • Supp Htg + Box Htg + HFR: The sequencer is in this state when the Zone Temperature is less than the Heating Setpoint, Box Priority = Supplemental, Supp Heating Control Status = High, and Box Heat Control Status = High.
  • Box Htg: The sequencer is in this state when the Zone Temperature is less than the Heating Setpoint and Box Priority = Box.
  • Box Htg + HFR: The sequencer is in this state when the Zone Temperature is less than the Heating Setpoint, there is no supplemental heat, and Box Heating Control Status = High.
  • Box Htg + Supp Htg: The sequencer is in this state when the Zone Temperature is less than the Heating Setpoint, Box Priority = Box, and Box Heating Control Status = High.
  • Box Htg + Supp Htg + HFR: The sequencer is in this state when the Zone Temperature is less than the Heating Setpoint, Box Priority = Box, Box Heating Control Status = High, and Supplemental Heat Control Status = High.
  • Prmy Clg: The sequencer is in this state when the Zone Temperature is greater than the Cooling Setpoint.
  • Temperature Unreliable: The sequencer is in this state when the Zone Temperature is not reliable.