The following table describes the attributes used by the Occupied Zone Sequencing (FC/AHU) module.
|
Name |
Description |
Default Value |
|---|---|---|
|
Cooling Control Status |
Indicates the status of the feedback controller for the cooling process. |
Overridden Set Name: Control Status |
|
Cooling Setpoint |
Contains the desired zone temperature when under cooling control. |
26 °C, 75 °F |
|
Fast Sequence Enabled |
Allows the user to enable or disable the transition to satisfied when the setpoint changes by more than the Setpoint Threshold. |
True |
|
Heating Control Status |
Indicates the status of the feedback controller for the heating process. |
Overridden Set Name: Control Status |
|
Heating Percent Cmd |
Indicates the current command from the heating controller that operates first. This signal comes directly from the PID in the output controller module. |
0.0 Display Units: % |
|
Heating Setpoint |
Desired zone temperature when under heating control. |
18 °C, 68 °F |
|
Setpoint Threshold |
Used to determine whether a significant setpoint change has occurred. |
1 °C, 2 °F |
|
ZNT-STATE (State) |
Indicates the current operational mode of the output controller. |
Satisfied |
|
Zone Temperature |
Contains the measured temperature in the zone. |
16 °C, 61 °F |