The following table describes the attributes used by the PID Tuning Reset modules.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Application Tuning Reset |
Provides a trigger to reset the tuning parameters of the PIDs in the output controllers. |
False |
|
|
PID Tuning Reset |
When set to True, signals the output controllers to calculate new tuning parameters instead of controlling. |
False |
|
|
State |
Provides the state to feed through State Selection to place the output controllers in the appropriate State Selection section to allow recalculation of the PIDs tuning parameters. |
Set Name: PID Tuning Reset |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)