Attributes (Humidification Sequencing) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The following table describes the attributes used by the Humidification Sequencing module.

Table 1. Humidification Sequencing Attributes

Name

Description

Default Value

Discharge Humidity

Contains the discharge air humidity.

50.0%RH

Discharge Humidity Setpoint

Contains the discharge air high humidity setpoint.

70.0%RH

Humidity Control Status

Value fed back from the humidification controller necessary for the sequencer to determine what actions to take. This input is the PID status from humidification output controller.

Normal

Set Name: Control Status

Humidity Process Variable

Contains the zone or the return air humidity.

50.0%RH

Humidity Setpoint

Defines the zone or return air humidification setpoint.

40.0%RH

HUM-STATE (State)

Current state generated by the AHU humidification sequence.

No Humid

Set Name: AHU Hum States

See Primary States (Humidification Sequencing).