Module Use in Applications (Application Mode Override) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Application Mode Override Uses in Application System Selection Trees
Module Instance Name Applications
AHU-Application Mode Override All Air Handling Unit Applications

To see a module's connections and how modules interact with it, view the Connections table.