Pass Through (Device Enable) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Device Enable Pass Through modules provide an automatic connection to the State Selection module. They typically take Network Inputs and connect them to State Selection. The Device Enable category’s Pass Through modules have the same configuration as the Pass Through category’s Pass Through (Boolean, Enum) module.