Reliability (Heat Recovery Enthalpy Suitability Determination) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Heat Recovery Enthalpy Suitability output is set to None if the OA Temperature, Exhaust Air Temperature, or the Low Limit Process Variable inputs are not reliable.