Availability Determination - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Availability Determination module enables or locks out a heating or cooling device. The module accepts as inputs outdoor air temperature, outdoor air enable setpoint, outdoor air enable differential, heating/cooling selection, network isAvailable, and a resolution mode. The module has a state output that indicates if the device should be enabled. When the output is True, the heating or cooling device is enabled. When the output is False, the heating or cooling device is not enabled.

You can view and modify the modules in this group’s logic.