Attributes (Tower Start Determination) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The following table describes the attributes used by the Tower Start Determination modules:

Table 1. Tower Start Determination Attributes

Name

Type 1

Description

Default Value

isAvailable

 

Indicates whether the system is enabled.

False

Pump Count

 

Indicates the number of active pumps.

0

Pump Delay

 

Indicates the amount of time to wait after turning off pumps before closing isolation valves.

20 Seconds

State

G

Provides an output indicating whether the cooling tower subsystem is enabled.

False

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)