The following table describes the attributes used by the System Enable modules:
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
HeatingCooling |
Determines the polarity of the comparison. Set HeatingCooling to Heating for a heating device, and set HeatingCooling to Cooling for a cooling device.If HeatingCooling is set to Cooling, a greater than comparison is used, so State is true if the OA Temperature is greater than the OA Temperature Setpoint.If HeatingCooling is set to Heating, a less than comparison is used, so State is true if the OA Temperature is less than the OA Temperature Setpoint. |
Cooling Set Name: Heating/Cooling |
|
|
HWSYS-AVAILABLE or CHWSYS-AVAIL |
Indicates if the State output is true when the device is available and is false when the device is not available. |
False Boolean |
|
|
isAvailable |
Enables or disables a device. |
True Boolean |
|
|
OA Temperature |
Indicates the outdoor air temperature. |
24, 70 Display Units: °C, °F |
|
|
OA Temperature Diff |
Indicates the differential for the setpoint. |
4 Display Units: °C, °F |
|
|
OA Temperature Enable Setpoint |
Indicates the outdoor air temperature setpoint above which, the cooling is enabled, or below which the heating is enabled. |
15, 61 Display Units: °C, °F |
|
|
Emergency Mode |
Enables pumps to start when there is a frost event. This is an input connected to the State output of the Frost Protection Determination module. |
Normal Set Name: CP Frost Protect |