Module Use in Applications (Plant Sequencing-Modulating) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Plant Sequencing-Modulating Uses in Application System Selection Trees

Module Instance Name

Applications

Modulating HX or Boiler Sequencing

Central Heating Applications

Secondary CHW Pump Sequencing

Central Cooling Applications

Secondary HW Pump Sequencing

Central Heating Applications

Variable Speed Fan Clg Twr Sequencing

Central Cooling Applications

To see a module's connections and how modules interact with it, view the Connections table.