Primary States (Plant Sequencing-Discrete) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
  • Control: Allows the output value to change, to meet the demand of the system.

  • Off: Indicates the system is disabled.

  • Pump Only: Allows a circulation pump to run as a minimum whenever the system is enabled.

  • System Interlock: Allows a global system interlock to be turned on prior to starting any stages.