Attributes (Plant Sequencing-Discrete) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The attributes in the following table are used by the Plant Sequencing-Discrete modules:

Table 1. Plant Sequencing-Discrete Attributes

Name

Type 1

Description

Default Value

Deadband

 

Indicates an area of a signal range or band where no action occurs and the State outputs a Hold.

2

Down Delay

 

Indicates the minimum time after a Stage Down that another operation (Stage Up or Stage Down) can be performed.

10

Display Units: Minutes

HeatingCooling

 

Inverts the action of the Stage Up/Stage Down.

Heating

Set Name: Heating/Cooling

Minimum Running Devices

 

Indicates the minimum quantity of stages to run.

0

Display Units: Minutes

Number of Devices Running

 

Indicates the number of devices that are currently being called by the BO sequencer to run.

0

Display Units: Minutes

Output

 

Indicates the number of devices that are being called to run.

0

Process Variable

 

Determines whether Stage Up or Stage Down is required by being compared to the setpoint.

100

Setpoint

 

Indicates the target value of the process variable.

100

Stabilize Delay

 

Prevents debounce in staging up or down.

180

Display Units: Minutes

Start-Up Delay

 

Prevents staging until the system reaches equilibrium.

60

Display Units: Minutes

State

 

Represents the current state generated.

Off

Set Name: Plant Sequencing Mode

System Enable

 

Enables the staging process to run using an Off/On command.

Off

Set Name: Off/On

System Interlock Status

 

Indicates the status of the Global System Interlock. The Global System Interlock Status must be On before any staging may occur.

On

Set Name: Off/On

Up Delay

 

Indicates the minimum time after a Stage Up that another operation (Stage Up or Stage Down) can be performed.

15

Display Units: Minutes

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)