Module Use in Applications (Plant Sequencing-Building Load) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Plant Sequencing-Building Load Uses in Application System Selection Trees

Module Instance Name

Applications

Boiler Sequencing by Building Load

Central Heating Applications

Chiller Sequencing by Building Load

Central Cooling Applications

Chiller Sequencing by Chiller Load

Central Cooling Applications

To see a module's connections and how modules interact with it, view the Connections table.