The following table describes the attributes used by the PID Sequencer modules:
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
BYP Saturation (Input 1) |
Provides an input that comes from the Cooling Tower Valve Control Status output. |
Disabled Set Name: Control Status |
|
|
CT Saturation (Input 2) |
Provides an input that comes from the Cooling Tower Fans Control Status output. |
Disabled Set Name: Control Status |
|
|
Delay |
Indicates the minimum time after a Stage Up that another operation (Stage Up or Stage Down) can be performed. |
15 Display Units: Seconds |
|
|
State |
Indicates the current state generated. |
Off Set Name: Plant Sequencing Mode |
|
|
System Enable |
Enables the staging process to run using an Off/On command. |
Disabled Set Name: Disable Enable |