Module Use in Applications (Count On Inputs) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Count On Inputs Uses in Application System Selection Trees

Module Instance Name

Applications

CHW Isolation Valve Status

Central Cooling Applications

CW Isolation Valve Status

Central Cooling Applications

Isolation Valve Status

Central Cooling Applications

To see a module's connections and how modules interact with it, view the Connections table.