Module Use in Applications (Dual Fan Alarms) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Dual Fan Alarms Uses in Application System Selection Trees

Instance Name

Application

Exhaust Fan Dual Alarms

AHU 100% Outdoor Air Single Duct Applications

Relief Fan Dual Alarms

AHU Mixed Air Single Duct Applications

Return Fan Dual Alarms

AHU Mixed Air Single Duct Applications

Supply Fan Dual Alarms

AHU Mixed Air Single Duct Applications

AHU 100% Outdoor Air Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.