The following table describes the attributes used by the Dual Fan Alarms modules:
|
Name |
Typeonr1558008170219.html#onr1558008170219__fn_b_bacnet_exposed |
Description |
Default Value |
|---|---|---|---|
|
Fan 1 Alarm |
This input represents the alarm condition of the first device. |
Default Value: Normal Set Name: Normal/Alarm |
|
|
Fan 2 Alarm |
This input represents the alarm condition of the second device. |
Default Value: Normal Set Name: Normal/Alarm |
|
|
Output - AND |
G |
This is the result of the AND operation. |
Default Value: Normal Set Name: Normal/ |
|
Output - OR |
This is the result of the OR operation. |
Default Value: Normal Set Name: Normal/Alarm |
B - BACnet Exposed Parameter, C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)